This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2576 - noise reduction for clear work with 35Mhz/2,4GHz Rx

Other Parts Discussed in Thread: LM2576, LM2596

Hello,

I'm trying to design a stabilized 5V on LM2576 (52kHz) for my lightning system.

35MHz Rx is connected to regulator linear BEC, regulator share the same battery as my module with LM2576.

Specyfications:
Input 5,5V - 21V (output may decrese below 5V when input is 5,5V - no problem)
max Iout 0,5A
On the output of LM2576 (after inductor) is ATmega8 wihich is switching on the darlington driver ULN2803 ports. Ports goes from driver to LEDs.
LM2576 works with inductor 470uH. Input Capacitors are tantal (tried 100uF to 680uF). Output capacitors are tanatal and electrolit (tried from 100uF to 3300uF - electrolits are LOW ESR JAMICON).
On the input wire I add small axial choke 0,33uH in series to minimize V ripple.

And I still get terrible noise (on the battery side). The noise on oscilloscope looks like around 40mVpp. But the servos rage when the Tx stands more than 1m (with antenna collapsed). I should easily go for a least 20m with no ripple. So my conclusion: the noise is from V ripple from wire system.
It seams like the problem is while the LED are blinking. The current goes instantly from 300mA to 500mA sometimes.

I get a little help from other RC forum to add ceramic capacitors 0,001 - 0,1uF.
And more to add common mode Toroid. But which one? On what frequencies or what uH should it have?

RC system is 35Mhz. Did not try on 2,4GHz, but if on 35Mhz will be ok, than on 2,4Ghz as well.

I would be very gratefull for help how to reduce the noise specially for this system?

I'm considering to use LM2596 with 150KHz switching - maby this is the clue?


Thanks
Maciek.
Poland/Europe

  • Hi Maciek,

    There are several things that you can do to reduce noise on a switching power supply.

    1) Look at your layout.  The placement of your input capacitor for a buck converter should be as close as possible to the drain of the high side MOSFET (VIN pin on LM2576) and the anode of the catch diode D1

    2) You state that you are using tantalum input capacitors.  The input is the noisiest part of a buck regulator with very high ripple currents.  Tantalum capacitors have a relatively high parasitic resistance (ESR).  This will cause a large voltage ripple at the input.  The ceramic input capacitors that were recommended (0.1uF) will help reduce the impedance at high frequencies, but you will probably need around 10uF of X5R ceramic at the input to reduce the fundemental of your noise. 

    3) If you you still need to lower the noise further after the above recommendations.  Consider adding more attenuation to your PI filter.  The addition of a common mode toroid is uneccesary as the noise from a buck converter is differential. However increasing the size of your choke to >100uF with some additional higher esr capacitors for damping could reduce your noise

    As a first pass try the following input capacitor design

     

    4)  You are correct that the high switching frequency noise of the LM2596 at 150Khz will be easier to filter.

     

    Regards,

    Marc

     

  • Hi Marc.

    In your example above, is this a filter design calculator screenshot or an application drawing you created?

    Thanks.

    Regards,

    David

  • 7288.Worksheet in Switching Power Supply Design_ EMI_Marc Davis-Marsh_09_03_13.xls

    This is a filter design calculator.  We made it as a first pass for the conducted EMI application note

    1256.snva489b_conducted EMI.pdf

    It doesn't take into account parasitics in the filter but it is good for a first pass.

    Regards,

    Marc