Other Parts Discussed in Thread: SM72441, SM72442, SM72445
As a reminder for people using the SM7244x devices:
- Output voltage limit can be modified on SM72442 and SM72441 by changing the voltage on pin A0 while the IC is running WITHOUT resetting the device
-Output voltage limit can be modified on the SM72445 by changing the voltage on pin A0 while the IC is running but change will be applied ONLY AFTER resetting the device
Output voltage limit works by reducing the duty cycle each MPPT step if the sensed output voltage (pin AVOUT) is higher than the set voltage limit (pin A0 or value set through I2C override).
Output voltage limit is enforced ONLY when the unit performs soft start and when running in MPPT, NOT when the "Panel Mode" switch is active (PM and PM_STARTUP state, as described in the datasheet)