Hi!
I am developing buck converter, which is able to operate at true 100% duty cycle. The input voltage can change from 10 to 34 Volts, but ouptut voltage is 12V (or equal to input voltage, when below 12V). As result I have chosen TPS40060 IC, because it has P-Fet, which provides mentioned d=100% operation.
At the moment I have made protoype of circuit on PCB, and with disabled UVLO and feed-forward function it's funcitioning OK from 14V to 34V input voltage. When input voltage drops below 14V, output voltage is decreasing. For example: at Vin=12.7, Vout=10.9; at Vin=11.6, Vout=10.0V; at Vin=10.5, Vout = 9.0V; At Vin=10V Vout=8.6V
How is it possible to obtain desired d=100% operation with TPS40060 IC ? (Should I do just readjusting of compensation network components, or there are possible other problems?)
(I already have design, which is properly operating at 100% duty cycle, based on LM5085, but unfortunately for higher power applications it's not suitable because LM5085 is not synchronous)