Other Parts Discussed in Thread: LM25119, LM5119
A customer would like to use LM25119 for a battery application at Vin=30V and Vo=16V, Io=20A or more.
(The load is battery.)
In a normal operation it is no problem.
But the voltage of Ramp pin will be almost 16V after operation stopped.(Because the output connect a battery.)
We are afraid that IC might be damaged.
How much the maximum absolute rating of Ramp pin is ?