Other Parts Discussed in Thread: TPS62360, INA219
Hi,
TPS62360 datasheet SLVSAU9C ties VIN and AVIN together on the 1st page, yet optionally put a 10Ohm low-pass filtering resistor on page 31 (fig 49) for noisy supplies.
1. The "functional block diagram" on page 9 shows AVIN is connected to a "Analog Circuit Supply" block, yet little information is found in the DS for this block. Could someone give a few comments on the purpose of this block, and the difference between VIN and AVIN? For example, is the Analog Circuit Supply modules used for "DCS-Control" or "remote sensing"?
1. From the use of 10ohm as LPF, it seems that the current goes into VIN is expected to be small (or efficiency would get very low). VIN and AVIN pins are tied together, and does this clue suggests that the VIN is the main power supply, and a much larger amount of current goes into VIN as compared to AVIN?
Matt