Other Parts Discussed in Thread: TLV62130, TLV62130A
What is the behavior of the TLV62130 under the following conditions:
a) the output is already under bias, at the programmed voltage, when it is provided input voltage.
b) the output is or goes above the programmed voltage.
c) the output is at some voltage and the input is zero.
The use case is feeding a 5V rail that may also be supplied by another source. I could not find discussion of this in the datasheet.
Thanks.