Other Parts Discussed in Thread: TPS61092, TPS61230
I'm using a TPS61092 in my design for various reasons, but I need load disconnect.
For some reason, the voltage on Vout is around 3.2V (Single cell LiPo input), even when the converter is disabled. Pulling the enable pin high does as expected and Vout jumps to 5V .. but I'm not sure why I'm getting 3.2V out of it (seems to be battery voltage minus a diode drop, perhaps?). I have stuck an LED on the output just to confirm it wasn't floating and the LED lights brightly, so it's definitely coming from somewhere.
Not sure if this works but here is my schematic, I don't really see anywhere else it could be coming from (USB is disconnected, so no Vbus).
dl.dropboxusercontent.com/.../Sheet1.pdf
I soldered the chip by hand using hot air at 250C. I'm wondering whether I perhaps managed to kill the load disconnect circuitry but somehow left the rest of it untouched, but I've done this many times before and never had an issue. Just odd.
Thanks