Other Parts Discussed in Thread: LM3481
Hi,
report AN-1484 "Designing A SEPIC Converter", but there is no information about that capacitors. I also check the schematic in the PMP1061 board and there is also the extra electrolytic capacitors.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM3481
Hi,
report AN-1484 "Designing A SEPIC Converter", but there is no information about that capacitors. I also check the schematic in the PMP1061 board and there is also the extra electrolytic capacitors.
Hello,
One design guideline to follow (mentioned in Section 10 for the LM3481 for the boost case) is to reduce the size of the high frequency current loop. For the Sepic that loop is highlighted in the following figure:
The main cause of noise in your circuit is the turnON/OFF of the FET. A simple way to reduce that noise would be to add a few ohms of resistance between the DR pin and the gate of the FET. Start with one ohm and see if you need to add more.
Placing a 1uF capacitor with low ESR on the output could also help filter out the high frequency noise.
If you have several scope probes connected in your setup, you might also be catching ground coupling noise on the scope that is not really present on the output.
Best Regards,
Florent Boico
Hello,
Also, please take note how you are measuring the vout ripple. Often long ground leads on the scope probe can present noise that really is not there due to "pick up" on the ground loop. To verify this is not happening, please make sure you are measuring directly across the cout capacitors with a very short ground lead. They have specialized spring clips that slide onto the barrel of the probe which will present a very short ground return for this very purpose. I hope this makes sense and helps?