Other Parts Discussed in Thread: SM72295
Happy new year Gents...,
I'm working on a new design and I'm using the TI SM72445EVM/NOPB reference design. I have a few issues:
1) The postage size SCH on page 7 of the AN-2241 SM72445 Evaluation Board DOC is way to small and impossible to read. I had the SCH enlarged but all the part #'s are fuzzy and unreadable. Can you please provide something I can read?
2) There are many "DNP" locations marked with an "X". I have no idea what the termination intent is for these connections. Example: U7, PIN 16, there is two "DNP" listed on that net. Where is PIN 16 suppose to connect to? Where is R71 supposed to connect to ? There many more similar "DNP" connections I confused about
3) There are a few parts on the BOM that can not be found on the respective manufacture's site:
L1 Inductor 20 μH EFD-30 core 1 Pulse Electronics PA2965.203NL
L2, L3 Choke, Filter 2 Pulse PA2972NL