Part Number: LM5117
Dear Employee
I have a question with the LM5117 application design by WEBENCH.
Input 24V(20V~30V)
Output 2V 12A
This media recorded the DCM change to CCM wave,the yellow line shaow SW and purple is IL.
We find LM5117 is unstable within Iout=1.6A~1.9A ,when up to 2A~10A or <1.6A,LM5117 switching node is stable.
Video
DCM Wave
CCM Wave
DCM to CCM Wave
In addition,the drive signal of the FET have ring,we want to know the ring's good status.
HO DRI & CURRENT @ Iout=10A
LO DRI & CURRENT @Iout=10A
Please kindly help to provide suggestion
Thank you very much