Part Number: TPS63020
All,
I have been working on a Solar Charger for my Internet of Things devices and am using the TPS63020 buck-boost converter to take the output of the LiPo battery or 6V (5.5V under any load) solar cell and produce a consistent output voltage of 4V. I have used WeBench to simulate this design. and am attaching the schematic and board layout sections:
Under no-load, the power supply puts out 4.08V but if I increase the load to 200mA, the voltage drops to 3.4V. I was careful to meet or exceed the specifications for the output capacitor and inductor. I have also confirmed that the input voltage is a constant 5.1V (Solar) or 3.75-4.2V (LiPo).
What am I missing or what information could I provide to help trouble shoot this? Thank you in advance for any advice.
Chip