Other Parts Discussed in Thread: TPS543B20, TPS549D22, TPS543C20, TPS548D22
Hi,
Let me talk about the maximum value of TPS53355 output current.
Customer use TPS53355 as the power supply for FPGA.
In evaluating the software of FPGA, the current became larger than assumed.
In that situation, I got two questions from customer.
1.Please tell me the risks of 36A of current and the output.
Customer understand the risk of package temperature (Tj).
Could you advise about other risks?
2.Is there a possibility of applying current protection other than Rtirp's current limit?
I understand that the overcurrent protection function can be set higher than 30A.
Could tell me about all the risks when outputting current exceeding 30 A including the specifications of internal FET etc.
Best Regards,
Yusuke/Japan Disty