I need to be able to operate this device at 125C ambient. I know the recommended Ta max is 85C.
Doing some power calculation I get that the max Pd is 0.41W at 125C
Pd = (Tj - Ta) / Rja = (150 - 125) / 60.7 = 0.41W
Next to find the max output current allowable at that temperature assuming 80% efficiency:
Pin - .41W = Pout
(3.3* Imax) / .8 - .41 = (3.3 * Imax) -> Imax = 496mA
If this is correct as long as I stay below 496mA Iout it should be OK,
Please confirm
Thanks