I am having trouble using the following schematic in actual implementation
When I try and run the device the system wont come up at 24V in I have to "ease" it in by first bringing it in at 10v and then turing the voltage up to 24v. additinally the switch frequency is way below expected (below 100kHz) and very unstable.
Also my target is to run the device at 100kHz but when I set the frequency setting resistor to 260k to achieve this, the device again has a very hard time coming up and have to ease it. The the frequency will slowly get to 100kHz as the device sits on, almost like its a thermal relation. once "warmed up" the device come on and off nominally.
Any help you can offer is greatly appreciated.