Part Number: LMR16030
Hi,
The datasheet in the design requirements (section 8.2.1 - Table 2) specifies a maximum input voltage of 60V,
but in the "Bootstrap capacitor selection" (section 8.2.2.7) specifies a 16V bootstrap capacitor. It's right?
My idea about gate charging of high side mosfet is that the Vgs voltage must be positive, so that the gate voltage
must be greater than source voltage, so the bootstrap circuit adds the output voltage plus the input voltage
to achive a higer voltage to charge the mosfet gate. So, the maximum voltage across the boot capacitor is at least
equal the input voltage.
So where is the error, in my idea of bootstrap circuit or in the datasheet?
Thanks in advance.
Geraldo Gomes.