Hi,
Our customer use LMR14030 to convert 12V to 5V, then convert 5V to 1.25V, at least 200mA as the core voltage of MCU by another DC-DC switching at about 1.2MHz. However, when MCU works, the inductor of LMR14030 has squeaking. If the 5V-1.25V DC-DC is no-load, the noise disappear. So I think the load current can cause noise of inductor, now what method we can do to eliminate this inductor noise?