Other Parts Discussed in Thread: LM2596, LM339, LM358
Dears ,There is a problem when i use lm2676 , I use the LM2676 as adjustable power , Vin=12V, Voutput 0.1V~10.0V, The Voutput could be adjust by the Voltage of LM2676 FB pin. The voltage of FB is through compare a adjustable duty cycle PWM and the LM2676 output , the problem is the Voutput will cutdown to 0 after 30s time ,please help to give some advice , many thanks !