Other Parts Discussed in Thread: TPS62821, TPS62671, TPS82671, TPS62801,
Hi,
I would like to use an output inductor with 1 μF,
but are there recommended values for output capacitors and other parts?
Best Regards,
Yuto Sakai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Chris-san,
Our customers place importance on efficiency as well as small size.
If they can put it on the board, They are trying to use an inductor with a slightly larger inductance value.
Therefore they are considering 1 μH.
Can you tell me that it is designed with a small size as the target,
but could you tell me the recommended value of peripheral components such as the output capacitor's capacitance value or the calculation method?
Best Regards,
Yuto Sakai
Hi Chris-san,
The conditions are as follows.
Vin = 3.3 V
Vout = 1.8 V
Iout = 500 mA
Best Regards,
Yuto Sakai