This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5165EVM-HD-P50A: Output Current too low

Part Number: LM5165EVM-HD-P50A

Dear Team,

could you please support with following issue I have with LM5165EVM-HD-P50A?

In the schematic I've modified R8 and R9 in order to reach a higher output current (see image below).

These are the values I used:

R8 = 47kOhm

R9 = 100kOhm

Based on my calculations, like this I expect to reach ca. 100mA of output current, but the board never goes above 65mA.

Can you please advise?

Thanks and best regards,

B