This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61291: About consumption current of Bypass Mode

Part Number: TPS61291


Hi,

I am considering creating circuits using TPS61291 devices.
The specification is below.
When waiting for the circuit, we plan to put the device in Bypass Mode.
I would like to ask about the supply current of VIN at that time.
In the data sheet, the current consumption of Bypass Mode is 15nA(typ).
Furthermore, in Bypass Mode, ILKSW is 10nA(typ).
If the load current is 10uA, the supply current of VIN is considered to be the following formula, is it correct?

IVIN = 15nA + 10nA + 10uA

(specification)
VIN : 3V (coin battery)
VOUT : 3.3V
IOUT : 60mAmax(operating), 10uA(standby)

Best regards,