I have designed for +-1.8 V for a 3V input from 2 AA bats.
I see 1.783 V at the +1.8V output and 0.315V at the negative LDO. The PGOOD signal goes high.
I see the same voltages when I don't give the EN-. However, the PGOOD signal is low as it should be.
I have tested rest of the circuit with the EVM to see if the load is creating some issue. The rest of the circuit worked fine with the EVM.
PFB my schematic and layout. Please do let me know how to solve this.