Other Parts Discussed in Thread: LMH6702, ADC08200
I have an operational amplifier (LMH6702) in my circuit that need to be powered with +/- 5V. Since I don't have a power rail of -5V in my circuit I used the LM2776 charge pump to obtain it using the +5V power rail available in my circuit. The LM2776 is not outputting the -5V that I was hoping for. The output is -1.76V it is not enough to power the operational amplifier. I followed the typical application of the LM2776 datasheet (http://www.ti.com/lit/ds/symlink/lm2776.pdf) using the same capacitor value. I am wondering if the 10uF tantalum capacitor (C39) on the -5V rail is causing this problem. The L3 choke is replaced with a 27 ohm resistor.
Excuse my english I speak french.