Other Parts Discussed in Thread: LM5170, LM5122
Hello
My customer has found a Boost type DC DC Controller capable of outputting 12V battery voltage input, output voltage 24V, Max output current 20A or more.
So I recommended the LM25122-Q1.
I have a few questions regarding the Maximum output specification for this product.
1. Is it possible to output 24V, 20A to the IC above?
2. Do you need special configuration (such as interleaving) for the above output?
3. Or is there a more suitable product than the LM25122-Q1?
Please help me.
Thank you
Best regards.