Part Number: TPS568215
Other Parts Discussed in Thread: TPS54302
Hello
I have a question for inductance selection of TPS568215.
I want to use an inductance as small as possible.
Then I tried to use 0.2uH (fsw=400KHz) for 1.2V out, but the control loop was not stable and 3.0V instead of 1.2V was output.
Using over 0.35uH seems to be good from my test.
Question 1)
I know there is recommended component values in the datasheet(Table 5 in SLVSDI8A).
But there is no information about possible inductance range.
Could you please tell me the smallest inductance value that can be used ?
Question 2)
I want to understand technical background of this selectable range for inductance value.
Is it impossible to open this kind of technical background information?
Regards,
Oba