Part Number: LM3488
Other Parts Discussed in Thread: LM5000, LM5002
Hi team,
Now I am designing a gas sensor circuit. In my circuit, I want to design 3.3V boost to DC40V ~45V voltage. Because I use 40V or 45V as the electrode voltage. When there is some VOC gas
in the electrode. The electrode can ionize the gas. Then it will generate the low current in the electrode. After this I will capture the low current signal with the op amp and ADC.
The low current maybe 1nA~1uA. So, now I need to output DC40V~45V voltage. Since my board size is very small. So I need the package of the DC-DC device should be the smallest. 3mm*3mm wii
be the best.
Q1: And I found LM3488 and LM378 can meet my requirement. Is this correct? If this is correct, can you send me the circuit?
Q2: Or you have any other ideas? Can the charge pump achieve my requirement?
Q3: Since my output current is very low. So the package of the inductance will be very small ,correct? If the package of the inductance is large, it will not good for my design.
For my above requirements, would you help me ?