This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217C Brownout issue @ Powerfail

Other Parts Discussed in Thread: TPS65217

Hi,

we have a Brownout issue with the TPS65217c, if the power supply is interrupted by a Powerfail e.g. ~150msec. the PMIC stands still in the OFF Mode, the nReset PIN and the PB_IN Pin has no influence!

I'm ussing the TPS65217c in the Battery-Less / 5V Operation mode (datasheet - 10.2.2.2) like the Figure 56 in the datasheet.

The AC Input is connected to the +5V Buck Controller and the USB Input is connected to GND, if i switch the INPUT form AC to USB - i see the 

same matter.

exist any Workaround for this matter or is this a know BUG ?

Thanks & Regards,

Sebastian