Other Parts Discussed in Thread: TMS570LS20216
Hi,
I'm using the TPS65381 connected to the TMS570LS20216. My code is based on the TPS65381/RM46_NoRTOS project. I had the TPS to go to the diagnostic state and watchdog function was running with respect to the watchdog fail count was always 7. At that time, I changed the DIS_NRES_MON (bit D2 in SAFETY_FUNC_CFG register) to 0 and the MCU was starting to reset. I couldn’t connect to the target because the MCU was resetting. So I externally connected 5V to the ERROR pin on TPS side to clear the error! (There is no pull-up on the ERROR pin in our circuit). Now I cannot connect to the target because of target power loss error, but MCU is getting the VCC and VCCIO correctly and the NRES (POR-RESET) pin is high.
Any help would be appreciated.
Regards,
Fatemeh