Part Number: TPS65911
Other Parts Discussed in Thread: TMS320DM8168
I have a TPS659112 that I would like to prevent sequencing while I program it over I2C for the correct sequence and voltages. Then when I am ready, I would like to initiate the sequence. I was originally trying to determine if I could use PWRHOLD or PWRON to prevent the device from starting up while I program it. After reading some other posts here, it seems like a better solution may be to leave BOOT1 floating, placing the PMIC in test mode, then programming everything over I2C. Is this the preferred method for accomplishing a "custom startup"? If so, what is used to initiate the sequence when I'm through programming?
I'm using a TPS659112 because I have two power systems, one is a daVinci PMIC and the other is for an FPGA, for which there is not currently a TPS65911x part. Since I will have Linux booted when I need the FPGA, it seems easiest to just program it at that point in software.
Thanks,
Steve