Part Number: TPS65094
Hi, I was looking at the formulas for calculating the needed inductors for the swich nodes. The datasheet seems to hint that the designs are optimizef for 0.47 uH inductors. Now, if I plug the data into the Intel Atom calculator (voltage/current) that gives me the result that I would need an inductor beyoned 0.47uH. Where do the 0.47uH come from? They are also in the reference design... Regards, Andreas