Tool/software: Code Composer Studio
Dear E2E:
From the datasheet of Tps65381A, I know that there are two ways to clear the IGN_PWRL bit.(put the device into standby state from active state)
1. A re-cranking on IGN pin
2. A detected CANWU wake-up event(send the WR_CAN_STBY SPI command)
In our system, the re-cranking on IGN pin cannot meet our requirements.And there is no CAN WakeUp Pin connect to the CANWU pin of the TPS65381.
Question:
Is there any other ways that I can clear the IGN_PWRL bit through the software?