Other Parts Discussed in Thread: TPS23753, CSD17527Q5A
Hi All
I'm using TPS23753 in the same configuration as seen in the TPS23753AEVM-235 circuit.
[http://www.ti.com/lit/ug/slvua27a/slvua27a.pdf]
However i'm not using the diode rectifier shown in the schematic, I'm using MB4S bridge rectifier. Rest of the circuit is the same.
For the transformer, I'm using Wurth 749119350 [katalog.we-online.de/.../749119350.pdf] instead of Coilcraft NA6223-AL with changes to pinout as shown below
|
Coilcraft |
Wurth |
|
3 |
5 |
|
4 |
6 |
|
1 |
3 |
|
2 |
1 |
|
10 |
10,11 |
|
7 |
9,8,12 |
|
6 |
7 |
For the output mosfet, i'm using BSC057N08NS3 instead of CSD17527Q5A.
Above alternatives have been proven to work and produce stable 5V.
I would like to know if there are any alternatives for input side mosfet FDS86244 and optocoupler TCMT1107.
Could anyone please confirm if I can replace:
FDS86244 with SI1480DH [http://www.farnell.com/datasheets/1760640.pdf]
or FDC8601 [http://www.farnell.com/datasheets/2000412.pdf]
or FDC3612 [http://www.farnell.com/datasheets/1639782.pdf]
Thank you for your assistance