If in the use case of TPS23751 (Type 1) and TPS23751 (Type 2) on the same board, can these VSS connect the same GND?
Or, are these VSS need to connect separate GND?
※Customer will use PoE Type-1 and Type-2 on the same board, and using TpPS23751 ×2.
Best regards,
Satoshi