This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2375: 12V/6W Reference Design

Part Number: TPS2375
Other Parts Discussed in Thread: PMP20531, PMP30290, TPS2373-4EVM-758

Hi, the PMP5595 reference design seems have the  ideal characteristics to power our PoE application. I am noticing in the schematic that the the connections to the transformer (T1) is different then some of the other reference designs.. e.g.  PMP20531, PMP30290.  Can anyone confirm that the configuration shown is correct? I want to connect the TD+/- and RD+/- pairs to our ethernet PHYS which is on the isolated side.

Thanks.

mike