This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD16570Q5B: Rds(on) Value in the SOA

Part Number: CSD16570Q5B

We try to calculate/get the Rds(on) value from the SOA of the D/S. However, we don't get the exact Rds(on) value from SOA curve and to match EC table.

For example, When the IDS is 400A and VDS is 0.4V, the Rds(on) should be 1mR. But in the EC table, the max. Rds(on) is 0.59 @10Vgs. is this correct?

1. How do you usually define the Rds(on) value in the EC table?

2. How do you draw the Rds(on) limitation on the SOA curve?