Hi,
We are working with this IC for already ~5 years. we are using full bridge topology with two of the IC driving a wireless charging coil. in our new design, the input voltage is 24V (was 19V before). Our Vdd is 5V (that being created from a DC-DC 24V input. buck converter. our SKIP# is 3.3V that being created from a 5V input buck (the same as the Vdd).
In our former design everything worked well, but now we see that sometimes that Driver will not start to work even when we invoke frequency and SKIP# is high (3.3V). We think that it might be related to the reason that our SKIP# is 3.3V that rises couple of uS after the 5V (Vdd), where in our former design the 5V was both the Vdd and SKIP# voltage. We think that this is might be related to your note:
We see that sometimes our Vdd voltage rises to ~2.5V before the 3.3V enable rises, so it might be that issue.
our uP connected only to the two PWM. we do not have any control over the enable (connected to pull-up).
I have 2 questions for that:
1. We are already in DV phase (already produce 400pcs), is there any way that we can turn the drivers on ? doing something with the PWM ?
2. For back up plan, we would like to connect the SKIP# to our uP with a Pull down of 50K ohms, and set the SKIP# to 3.3V after uP turns on. Do you see any problem with that ?
This issue is urgent, so I will happy if you can assist us ASAP
Thanks
Amir