Hi,
My customer would like to confirm if the LSET pin of CSD95480, CSD95481 can be left floating?
Best regards,
Randy Chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer would like to confirm if the LSET pin of CSD95480, CSD95481 can be left floating?
Best regards,
Randy Chen
Hi Randy,
LSET pin can not left floating. Please see use the datasheet graph to determine LSET resistor based on your inductor selection.
Regards,
Weidong
Hello,
LSET pin can't be left floating on theCSD95480/95481. Customer needs to use the Data-sheet equation and determine the LSET resistor value based on Output Inductor they use. Should be resistor pull-down to GND configuration.
Hi Lucian,
Can you specify more detail about the LSET function and the impact if it’s floating?
Is it work abnormal with TI’s controller if floating, please advise? Thank you.
Best regards,
Randy Chen
Hi Randy,
LSET is used to pin strap the inductor value during power on to center the current sensing circuitry in the appropriate range for the application. If it is not set correctly, the current sensing circuitry will not behave correctly and will be inaccurate. Since the current sensing signal in a typical application is used as part of the control loop, this signal is considered critical to the design. Therefore, there is open-pin detection built into LSET that will flag the controller that there is an issue by holding TAO low if LSET is left floating. Other than TAO being held low, the power stage will continue to respond to PWM inputs so it is up to the controller to protect the system. You need to check the specific controller you are using to determine if it will correctly interpret the TAO low as an issue and prevent startup.
Best Regards,
Evan Reutzel