Other Parts Discussed in Thread: ISO124
I get no output from multiple devices.
Do I need an output load?
Do I need to do anything with the SYNC pin?
Are any caps required for a bench test?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I get no output from multiple devices.
Do I need an output load?
Do I need to do anything with the SYNC pin?
Are any caps required for a bench test?
Thanks
Michael;:
DCP02 series including DCP022415DP requires a minimum 0.47 µF input ceramic capacitor with 1.0uF ceramic capacitor on each output to ground. Does this application have any connection o n the input sync. pin to ground? or any stray capacitance greater than 3-5pF on this pin?
What is the current rating on the input 24V power source?
What is the general secondary application? is it a IGBT drive circuit or FET driver with high voltage on the secondary ground( com ?
Contact me directly at tguerin@ti.com on your response? Also include, if possible your tel. # in this response.
Tom
thanks for that I will try the cap today
No connection connection to sync pin.
The supply is 10A.
The application is "isolated supplies for ISO124 devices"
Michael:
Thanks for the information on DCP022415Db using the ISO124 . DCP022415 when it has no load on each ± output can be as high as 30V . Is there a voltage difference between primary and secondary isolation grounds of > 42VAC or 60VDC?
Can you sent me an e-mail so we can discuss this application.
Tom