Hello,
Our customers use the following capacitor in parallel as an output capacitor of the LMZ31710.
These are different from the recommended capacitors.
Are there any problems?
・T520D687M004ATE012(KEMET) 680uF ±20%,ESR 12 mOhms (100kHz 25C),T520
・C3225X5R1A476M250AC(TDK) 47μF ±20%,ESR 2.4mOhms (100kHz),X5R
・C1005JB1A105KT(TDK) 47μF ±20%,ESR 2.4mOhms (100kHz),JB
・C1005JB1H104K050BB(TDK) 100nF ±10%,ESR 227mOhms (100kHz),JB
Vin=5V,Vout=1.05V
Best regards,
Seishin