Other Parts Discussed in Thread: LMZ31710
Hi, team.
Can LMZ22010 be used which the external clock synchronous function is changed during operation?
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kobayashi,
Denislav and me took two measurements. The first one is switching from internal clock to a lower frequency external clock(~250kHz), the second one to a higher frequency external clock (~500kHz).
The Graph shows you the external clock signal and the behavior of the inductor current and the output voltage on this "transient". It needs about 20 cycles to stabilize to the new frequency. You can expect about 50mV of transient on the output ( depending on the step in frequency).
Have a nice day,
Michael