Other Parts Discussed in Thread: DCR021205
Hello.
I'm designing a circuit and I want to add TWO DCR011205. I want to know if is it possible to connect both outputs (VOUT+) to have all the output current available in one single line of 5V. Each DCR011205 provides 200mA of output current and I want to have the 400mA (both outputs in shortcircuit) in a single line...is it possible?
Thank you.