Other Parts Discussed in Thread: TPS62135
I'm using TPS82140 to convert a 12 V rail to 5.7 V, and the load will be drawing roughly 0.5 A from the 5.7 V output. I do get the right output voltage but the switching frequency I measured is about 500 kHz, which is far off the 2MHz nominal switching frequency. I need the switching frequency as high as possible because I'm using it to supply a 13 GHz VCO and I have spurious requirement below 1.5 MHz offset. The only thing I did different from Figure 5 of the datasheet is the R1 and R2 values. I've used R1 = 51 kOhm and R2 = 8.2 kOhm to set the output voltage. Is the R2 I used too small so that it messed up the switching frequency?