Hello,
resistors recommended for the application schematic for Vout = 2.5V (Figure 25 on page 18 of the datasheet SNVS677F rev. F from Nov-2014) does not correspond to equation (5) on page 14.
The 118k is recommended for RB (along with 150k RT), however when the RB is calculated using equation (5) it results in 111k only. Top and bottom resistors recommended for the other three application schematics (for 1.2V, 1.8V, 3.3V) match well the equation (5). It looks like to be a typo or copy&paste error.
Please double check correctness of the 2.5V application schematic and confirm that it is really an error. Or am I missing anything?
Best Regards,
Josef