Hi
I am using the LMZ30606RKG. I haev a question about the layout of the AGND and PGND.
- according to TI support engineer I should have connected the PGND and AGND in schematics. thing is, in the datasheet layout examples it shows two separate planes of the AGND and PGND.
so my question are:
- if I do not separate them in schematics. do i ignore datasheet layout recommendation which shows two GND planes?
- if I do separate them, how do i deal with pin 37? in the datasheet figure 36, pin 37 is in the middle of AGND but no separation