In current application guide, it only talks about current sharing when the input and output voltage is the same. But is it possible to use different voltage input? In fact, I have two voltage sources having almost but not exactly the same voltage, and I would like to put each of them into a LMZ31710 to combine them into one voltage source. Is that possible?