Hi,
I have a question on the TPS3511 regarding PGin and the undervoltage lockout feature.
When the TPS3511 is enabled by %PS_ON the delay for undervoltage protection is 75ms.
This is enough time for all the powersupplies (12V, 5V and 3.3V) to start-up.
The supervisor also has a PGin to disable PGout and undervoltage protection fast in the event of input power failure.
However when the PGin goes high again the undervoltage protection delay is only 3.2ms (minimal)
This seems short to ramp up all the powersupplies of a ATX powersupply, am i misintepreting the use of PGin or is this short power-up time intended?
best regards,
Tom