Dear all,
When I actual test UVOV value to TPS3700, I find a problem.
1.The monitor voltage is 4.706V(The output state 1 change to 0), When the monitor voltage form under voltage to normal;(There is no floating)
2.The output state is floating when monitor voltage form normal to under voltage;(Monitor voltage range:[4.649V,4.669V]
3.The monitor voltage is 5.399V(The output state 1 change to 0),when monitor voltage form normal to over voltage;(There is no floating)
4.The monitor voltage is 5.321V(The output state 0 change to 1),when monitor voltage from over voltage to normal.(There is no floating).
I want to know why is there floating state when the monitor voltage form normal to under voltage?? And there is no floating state at the other transfer.
Thanks!