Other Parts Discussed in Thread: LMR14030, , LM2596, TPS53353
I am trying to protect my LMR14030 DC/DC converter set to 3.3V and as well the 12V bus. The protection i made on the input side of the converter using TPS25944L.The idea is to protect also the 12V Bus where the converter is supplied from, also in case if the LM14030 gets an internal short/ LOW Side + High Side switch/ or whatever.
My assumption was so that I know the let say nominal steady state input current of the converter, so if it goes double to high in case of overload at the output or in case of internal shorts then TPS25944L will switch-off the circuit. I need a latch function. Everything works fine if I am increasing the load at the output. I change the load (of the LMR14030) till the trigger point (my case 0.75A input of TPS25944 corresponding to 1.85A at 3.3V output).
Now is the problem. I have external reset-er which is periodically resetting the TPS25944 if there is a Fault flag.
So the problem occurs if there is a still to heavy load at the output and the TPS25944 was commanded to start.
It is starting and if to heavy load still exist the whole circuit is oscillating and consuming power from the 12V bus. This must be avoided, if failure at the output it must try periodically to turn on the converter with the load, but after certain time 4ms must be off.
Circuit is oscillating for the load between the trigger point and the full metal short.
The question is how to keep the circuit off so long until there is an overload(over the trigger value) or short?
The TPS25944 is not switching off when its seeing short pulses, shorter than 4ms and integrator of those pulses would be very useful. It should try to turn on the LM14030, but as soon as it recognize overload conditions should goes off (after 4ms). There is somewhere a closed loop and its self oscillating.
I enclose the picture the Pink is output Voltage from the TPS25944 ( Input was 9V from DC power supply limited to 1.25A average current from DC meter was about 0.4A).
Yellow is an Input current taken from Imon Pin (at R 20k to GND, its about 0,5A /0,5V). EN Pin of LMR14030 was pulled up to Vin to be sure its not a problem.
regards