Hello,
I am designing the 26601 into a product and have been doing some testing with the 26600 EVM kit.
When I test the trip values on the board with the included Rilim values, I seem to be getting trip currents that vary from the stated range in the data sheet.
Some examples:
R = 60.4k, Calculated current 0.2A, tested 0.167, EVM stated value 0.2A.
R = 12.1k, Calculated 1.0A, tested 0.92A, EVM stated 1A, Data sheet spec 0.95-1.05A
R = 8.06k, Calculated 1.5A, tested 1.29A, EVM stated 1.5A, Data sheet spec 1.425 - 1.575A
R = 5.36k, Calculated 2.2A, tested 2.11, EVM stated 2.23, Data sheet spec 2.11 - 2.35A
Cases for R = 60k, 12k, and 8k seem to be off from the guidance in the data sheet and the EVM manual. I am particularly interested in the R= 60k condition since I intend to limit output current to 0.2A.
Are these deviations part of the expected variation for this part? If so, is this repeatable, e.g. if I use a resistance that gets me a threshold of 0.2 amps on the EVM kit, will my current limit be repeatable at 0.2 amps within 5% (or some %) for future chips? If not, this suggests +- variations approaching +-20%. What is the actual variance I can safely assume?
Thanks,
Mike