Hi,
I was using the Ic's TPS22963C(to generate VCCAUX_1V8 from 1V8)and TPS7A8300RGWT (to generate VMGTAVCC_1V and VMGTAVTT_1.2V from 1V8).The
EN pin (of TPS7A8300RGWT) and the ON pins (of TPS22963C) were driving from the PIC(3.3V) and the pins were used as the power sequencing
pins to power ON the Ic's(as per the enable sequence).
Now we are planning to power ON the supplies without programming the PIC.We are going to provide pull ups to EN and ON pins.We referred the
datasheets to check whether we can provide 1.8V to EN pin and ON pins(since the PIC pin is driving 3.3V ) with pull ups or not? (There are no translators in between the devices)
Thanks in advance
Sreelakshmi