Part Number: LM25066
Hello I have LM25066EVK. The shunt was changed to 10mOhm ( stock 0,5mOhm) to gest 2.5A current limit at Vref 25mV. Configuration of the board is as follow: CL to GND, CB to GND, RT to GND.
Vin 12V from DC power supply limited to 5A and I perform hard short circuit on the output. So few question to the experts.
What I see is that during limitation period (about 8-9ms) current is limited to about 0,5A not to 2.5A.
1. Why is it so, why not 2.5A?
I enclose screen.
2.The first peak is about 3.5 Amps - why there is such peak about 400us long?. Is my shunt 7mOhm or Vref 35mV?
Pink is current 0.5A/div Yellow is the gate voltage refered to the Vout(Drain).
Power limit is never exceed 3.5A x12V gives about 42W (LM25066EVK spec 80W)